LTE TDD
This topic describes carrier assignments and related settings for Waveform Playback (ARB) capability.
Carriers of Waveform Playback Capability
Maximum Number of Carrier Allocation
Adds a new component carrier into waveform. In the GUI, new carriers are added at the top of carrier list.
The maximum number of carriers is 16.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier:ADD TDDULEUTRA|TDDPRACHEUTRA|CW|TDDDLADVANCED|TDDDLULBASICA |
|
SCPI Example |
:RAD:LTET:WAV:CCAR:ADD TDDULEUTRA |
|
Notes |
Set only TDDULEUTRA = Advanced TDD Uplink E-UTRA; TDDPRACHEUTRA = TDD PRACH E-UTRA; CW = Continuous Wave; TDDDLADVANCED = Advanced TDD Downlink; TDDBASICA = Basic TDD UL-DL. The maximum number of carriers is 16. |
|
State Saved |
No |
|
Preset |
– |
|
Range |
Uplink E-UTRA | PRACH E-UTRA | Basic TDD UL-DL | Advanced TDD Downlink | Continuous Wave |
|
Initial S/W Revision |
A.14.00 |
| Modified S/W Version | A.20.01 - Added Basic TDD UL-DL and Advanced TDD Downlink |
This table shows supported carriers on PWSG LTE and mapping information to carriers of Signal Studio LTE.
|
Carrier Name |
Referenced carrier of Signal Studio |
Notes |
|---|---|---|
|
Uplink E-UTRA |
LTE-A TDD Advanced TDD Uplink CA Advanced LTE-A TDD Uplink CC |
Only Uplink carrier can be added after Uplink carrier is already assigned, except Basic carriers |
|
PRACH E-UTRA |
LTE-A TDD Basic TDD PRACH-CA Basic LTE-A TDD PRACH CC |
Only PRACH carrier can be added after PRACH carrier is already assigned, except Basic carriers |
|
Continuous Wave |
CW Carrier |
|
Refer to each carrier section for more details of each carrier.
Click "+" button to add a carrier.
The carrier selection menu indicates the following structure and labels.
Uplink (CA) [ARB]
Uplink E-UTRA
Uplink (CA) [Real-Time] (Fixed configuration for Real-Time)
Uplink E-UTRA
PRACH (CA)
PRACH E-UTRA
Downlink (CA)
Advanced Downlink
Basic TDD CA
Continuous Wave
The following carrier configuration is allowed on Waveform Playback [ARB] capability.
1 CA carrier (Uplink CA or PRACH CA) and maximum 15 Continuous Waves or
maximum 16 Continuous Waves
For Real-Time Uplink capability, one fixed configuration available.
1 CA carrier
5 Uplink E-UTRA component carriers can be added in an Uplink CA with Waveform Playback capability.
1 Uplink E-UTRA component carrier is configured with Real-Time Uplink capability. Add or delete carriers are not available on Real-Time Uplink capability.
5 PRACH E-UTRA component carriers can be added in a PRACH CA.
This setting deletes the specified carrier. The carrier is specified by the carrier number, starting from 1.
Click "-" button to delete the specified carrier. The identifying numbers of subsequent carriers are adjusted automatically.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier:DELete <integer> |
|
SCPI Example |
:RAD:LTET:WAV:CCAR:DEL 1 |
|
Notes |
Set only |
|
State Saved |
No |
|
Preset |
– |
|
Min |
1 |
|
Max |
Valid carrier number: 1 to the maximum number of carriers |
|
Initial S/W Revision |
A.14.00 |
SCPI only, Query only.
Returns the number of configured carriers. A component carrier is counted as 1.
|
SCPI Command |
[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier:COUNt? |
|
SCPI Example |
:RAD:LTET:WAV:CCAR:COUN? |
|
Notes |
SCPI only, Query only |
|
State Saved |
No |
|
Preset |
1 |
|
Initial S/W Revision |
A.14.00 |